6/27/2013 2:43 PM | |
Joined: 7/12/2012 Last visit: 7/10/2023 Posts: 10 Rating: (0) |
Yes I have connected 24V. Am in a dead end here. Any ideas? |
6/27/2013 4:20 PM | |
Joined: 4/24/2006 Last visit: 9/13/2024 Posts: 8736 Rating: (1168) |
Hello eliasd, Let's try something else. The CPU has two connectors. The one at the left is for Analog I/O and last byte of Digital inputs (the one you can read in) The second connector at the right is for Digital Inputs and Outputs. (Left are inputs and right are outputs) Can you confirm you are using the right connector (X12) At the attachment you will find the wiring. (page 21) Best regards, Wizard Attachments7300_cpu314c_2_pndp_product_information_en-US_en-US.pdf (139 Downloads) |
Follow us on