7/5/2007 10:17 AM | |
Posts: 5822 Rating: (412)
|
Yes, because it is connected to both PLCs than. Best regards J_Bell |
7/6/2007 10:23 AM | |
Posts: 5822 Rating: (412)
|
Hello Sadd, where do you read the data from, from the Master or really from the Slave? Best regards J_Bell |
7/17/2007 6:42 PM | |
Posts: 11 Rating: (0) |
Using Protool the connection was set to the Slave not the master, I had 3 connections in the Protool projectone to the master and 2 to the salves I had 2 slave doing motion contol 2 axis per slave then I also had IO mapped to the master slave for real time control.(the connection was set as routing). SADD AttachmentRouting.pdf (570 Downloads) |
Follow us on