Industry Online Support
Technical Forum
7/30/2013 11:38 PM | |
Posts: 3 Rating: (0) |
Hello, I have a system which is running ok andI wish to add 2X AI and 1X AO at a distributed module withthree spare slots. Configuration is: 315-2 DPCPU (6ES7 315-2AG10-0AB0) connected with profibus to ET200L-SC 32DI(6ES7 131-1BL11-0XB0) TB 16SC(6ES7 120-0BH01-0AA0) expansion fitted with: 4 X 2DO(6ES7 122-1BB000AA0) 1 x 2DI(6ES7 121-1BB00-0AA0) The problemI am having is when I fit : 1 X 2AI(6ES7 123-1GB10-0AB0) 1 x 1AO(6ES7 124-1GA00-0AB0) WhenI load the HW, both BF and SF leds are on, if i remove the Analog cards from the HW and reload all is ok. I was wondering if the cpu firmware maybe the issue V 2.0.8 I have attached the hardware in an empty project, the module i wish to modify is profibus address 7 AttachmentProblem_.zip (182 Downloads) |
7/31/2013 12:51 AM | |
Posts: 3 Rating: (0) |
added CPU diagnostics
AttachmentDiagnose5.zip (161 Downloads) |
7/31/2013 2:30 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating: (709) |
Hi Pob, Look at page 2-13 try to see the manual it seems that you can not put them as you wish, if you want to try .... Dezentrales Peripheriegerät ET200L, ET200L-SC und ... - Siemens Hope this help |
Follow us on