9/12/2014 3:17 PM | |
Posts: 1 Rating:
|
hello,,,,, AttachmentD:\Temp\315-2dp.pdf (95 Downloads) |
Last edited by: Min_Moderator at: 9/12/2014 3:20 PMAttachment reattached |
|
9/12/2014 3:30 PM | |
Joined: 1/21/2013 Last visit: 4/21/2023 Posts: 4617 Rating:
|
Hello GA_20, For me you need 3 DP/DP Coupler or between Master Yellow and Green or between Pink and Violet and remove the row of the DP / DP coupler between the Yellow and Violet Pay attention to how much data you can exchange with the DP / DP Coupler Function: The function of the DP/DP coupler is to connect two Profibus DP networks with one another and to transfer data between the masters of both networks. The maximum size of the transmitted data is 244 bytes of input data and 244 bytes of output data. The DP/DP coupler can be configured with STEP 7, or with a configuration tool and a GSD file. Features: The DP/DP coupler has the following features:
New DP/DP Coupler Released for Delivery - Siemens Industry ... |
Last edited by: Ste39 at: 9/12/2014 3:53 PMAdd note Last edited by: Ste39 at: 9/12/2014 3:32 PM |
|
Follow us on