7/8/2019 10:27 PM | |
Joined: 7/18/2017 Last visit: 2/17/2022 Posts: 1 Rating:
|
Hello, I am having a similar issue. I have created a new PLC Project in TIA Portal 14. This PLC is to communicate with other PLCs to gather and send data. PUT / GET seemed the easiest. The "Master" is a 1516 3PNDP. I have created the networks for communication to another 1516 which also uses TIA14, and to a 315F-2PNDP which is also in TIA14. The communication works properly here. The problem now is that I am trying to communicate to a 317F-2 DP which is programmed in Step 7 V5.5. It is using a CP 343-1 Lean card to communicate. I can use the existing ethernet lines and go online with the 317 PLC without issues, but the 1516 cannot communicate with it. Any help appreciated ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/09/2019 10:46:09New subject after splitting |
|
7/9/2019 11:44 AM | |
Posts: 3093 Rating:
|
Hello, How do you evaluate the status of system blocks in STEP 7 (TIA Portal)? Regards, |
Follow us on