7/26/2024 5:17 AM | |
Joined: 1/21/2013 Last visit: 8/15/2024 Posts: 3044 Rating:
|
Hi, Congratulations on your first post. In the future, I would like you to post only one question per topic, this would make it easier to answer and for others to follow the topic.
Could you please describe your requirements in more detail? To be honest, I have no real idea what you want.
In WinCC Unified the parameters of the screen elements can be dynamized in different ways. If you want to change the color on a click, you would have to use "press" and "release" events. There you can program some small scripts like:
To get a login dialog on a user action, you need to configure some users with different roles and assign some function rights to the roles. For a screen object, configure a function right on the "Authorization" property ("Security > Authorization"). If the active user does not have the required function right, a system-defined logon dialog will appear, asking for some user credentials. For more information, see "Configuring user management in the engineering system for Runtime" in the system manual. Kind regards |
This contribution was helpful to
2 thankful Users |
7/30/2024 1:28 PM | |
Joined: 7/30/2024 Last visit: 8/16/2024 Posts: 70 Rating:
|
For easier commuincation and a better chance of getting usefull answers, only ask one question per Post please. The three questions from this post have been split up into seperate Topics. 1. How can be add a field that updates dynamically the screen path on wincc unified panel - MTP1500 - Tia portal V17? This question can further be discussed here. 2. How can we change the color of the switch when clicked on wincc unified panel - MTP1500 - Tia portal V17? This quesiton can further be discussed here. 3. How can we add a login pop up similar to what we have in TP700 on wincc unified panel - MTP1500 - Tia portal V17? The final question can further be discussed here. Kind regards, Lan_Moderator |
Last edited by: Moderator_Lan at: 07/30/2024 13:33:24Last edited by: Moderator_Lan at: 07/30/2024 15:13:50split into multiplie topics Last edited by: Moderator_Lan at: 07/30/2024 15:27:01closed because of splitting into seperate topics |
|
Follow us on