Industry Online Support
Technical Forum
11/8/2012 6:48 AM | |
Joined: 1/25/2011 Last visit: 1/25/2022 Posts: 1 Rating:
|
I have a problem that is T-CPU and IM174 for stepper mode without encoder. Problem is Pulse output is too smaller then setpoint. Please refer to attached Jpg image file that is control panel include my problem. It is actual speed is too small and also following error is getting bigger but it hasno encoder. also I referred the FAQ in this site about this. FAQ:How must you parameterize the IM 174 in combination with the Technology CPU or SIMOTION when steppers are to be addressed without encoder feedback?ID: 48203982 https://support.automation.siemens.com/WW/adsearch/resultset.aspx?region=WW&lang=en&netmode=internet&ui=NDAwMDAxNwAA&term=steeping+im174&ID=48203982&ehbid=48203982 Please let me know. What is my mistake? |
Last edited by: Peter143 at: 11/8/2012 8:53 AMLast edited by: Peter143 at: 11/8/2012 8:21 AMLast edited by: Peter143 at: 11/8/2012 6:53 AMLast edited by: Peter143 at: 11/8/2012 6:51 AM |
|
Follow us on