9/4/2024 9:18 AM | |
Joined: 1/9/2019 Last visit: 10/3/2024 Posts: 2 Rating: (0) |
Hello, I have one problem with MB_SERVER on CP 1243. I used this configuration sometimes and it works, but if I disconnect ethernet cable and I reconnect after few seconds, the communication doesn't start and status remains to 7006. The only way to restart the communication is turn off 24V DC power supply and turn on again. Stop/start CPU doesn't have effect, the status of MB_SERVER in this situation is 7002. Someone can help me? Thank you very much ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/04/2024 09:42:31New subject after splitting |
|
Follow us on