8/21/2008 4:15 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, 1) Are you sure that the switch is really a switch and not a hub? If it is a hub, the bandwidth is shared among all devices on the network. 2) You can see if the CP has 100 Mbps and full-duplex either via the LEDs on the CP or in the NCM diagnostics. One possible way to start the Diagnostic is: HWConfig ==> sect the CP ==> Tab diagnostic ==> start diagnostic. For the PC, in network connections, you can see the status of the interface and check the speed. 3) You could also use a tracing tool like wireshark (www.wireshark.org) to measure - the traffic on a given port of the switch (please activate port mirroring) - the broadcast load on the network |
Best regards |
|
8/22/2008 11:05 AM | |
Posts: 5822 Rating: (411)
|
Hello, is it possible that you have a CP 443-1 EX11? If so I would strongly recommend to upgrade the CP to the latest version V 2.7.3. You can find the firmware at: CP 443-1 Firmware Update V2.7 and Unrestricted Use on Every Hardware Release (6GK7443-1EX10-0XE0 and 6GK7443-1EX11-0XE0) I hope this will help. Best regards J_Bell |
8/22/2008 12:57 PM | |
Posts: 5822 Rating: (411)
|
Hello, please let me try to answer your questions: J_Bell |