3/14/2013 3:10 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Saga, Have a look: SIMATIC S7-300 Outdoor DC/DC-Stromversorgung 6ES7 305 |
This contribution was helpful to1 thankful Users |
3/16/2013 12:25 PM | |
Joined: 11/8/2011 Last visit: 8/21/2024 Posts: 387 Rating: (43) |
SIMATIC S7-300 Outdoor DC/DC-Stromversorgung 6ES7 305HI ste39whether is there any DC DC covertor with 5A available in the above link only it has 2A |
3/16/2013 7:54 PM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839)
|
HI ste39 whether is there any DC DC covertor with 5A available in the above link only it has 2A Hello, 24VDC, 2A is the max. current you can get from SIEMENS DC/DC converters if your input is 48 VDC. Here's bellow link for all SIEMENSDC/DC converters
|
Last edited by: Ayman Elotaify at: 3/16/2013 7:55 PMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
3/18/2013 6:08 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hi Saggy, Look this: DC/DC converters - QUINT-PS/24DC/48DC/ 5 - 2320128 and Assembly adapters - QUINT-PS-ADAPTERS7/1 - 2938196 Hope this help |
Last edited by: Ste39 at: 3/18/2013 6:21 AM |
|
3/18/2013 7:01 AM | |
Joined: 11/8/2011 Last visit: 8/21/2024 Posts: 387 Rating: (43) |
thank you |
Follow us on