Industry Online Support
Technical Forum
6/14/2009 8:54 AM | |
Posts: 557 Rating: (64) |
hi i think you go with profibus to OLM protocal.(fibre optics link).so you can achive this task.(5KM) Find the link, hope this will help.......... Configuration rules for "10-Mbit shared LAN" (transceivers, OLMs, etc.) SIMATIC NET Twisted-Pair and Fiber-Optic Networks http://support.automation.siemens.com/WW/view/en/14650423 http://support.automation.siemens.com/WW/view/en/27069465 http://support.automation.siemens.com/WW/view/en/8763736 regards |
Last edited by: Eastern at: 6/14/2009 8:58 AM |
|
6/15/2009 1:55 AM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (309) |
Hello, Just to comment on number of connections. I think the number is just 57 not 57*2. In SWR, only oneconnection is configured in WinCC and a C script is used to switch between the 2 PLCs by changing IP address but still on the same connection. However, 57 connectionsare still representing a very big communication load. The solution proposed by Daga is very good. CPUs dedicated for communication are recommended in such cases. Best regards. H-H AttachmentSWR_WinCC_Connection.pdf (393 Downloads) |
This contribution was helpful to1 thankful Users |
6/15/2009 10:47 AM | |
Joined: 2/26/2007 Last visit: 12/12/2024 Posts: 16 Rating: (1) |
Dear friends, Thanks for ur reply. I am going to workoutmy configuration based on daga's suggestion. |
Follow us on