8/5/2022 4:31 AM | |
Posts: 3 Rating: (0) |
thanks for your support i finally connect to the CUD with STARTER and the drive work already but can you please help me to know how to reverse the rotation ( which parameter is used) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/08/2022 09:35:07New subject after splitting |
|
8/8/2022 1:45 PM | |
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating: (1) |
Hi Fagbe, Direction of rotation reversal using field reversal
Binector = 1 A negative field direction is selected. Changing the logical level of the binector controlling the function "Direction of rotation Field reversal is completely executed. Level changes at the connector input have no effect Regards
|
If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
|