12/17/2019 4:44 AM | |
Joined: 3/19/2010 Last visit: 4/27/2022 Posts: 3 Rating: (0) |
I am using 6SE7021-0EP50 with options C13(encoder) + G91 (communication board). This drive has a rated current of 10A & peak current of 30A. This is used for positioning in bar handling area. I want to replace this with Sinamics Drive. Which drive should I select. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/17/2019 11:28:20New subject after splitting |
|
Follow us on