Industry Online Support
Technical Forum
10/7/2024 1:42 PM | |
Posts: 2 Rating:
|
Good morning, I have a mod. IP 6SL3210-5FE10-8AU0 drive that does not turn on the display but the RDY and COM LEDs light up with a certain code. The ready lights up solid red, then the com flashes orange three times, then they both flash red with a frequency of about 1Hz. I imagine it is a code, as I said, but I do not understand what it is. Does anyone have an idea? Thanks to anyone who answers me. Regards. Roberto p.s. the display does not turn on. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/07/2024 13:54:56New subject after splitting |
|
Follow us on