Industry Online Support
Technical Forum
6/12/2012 7:28 AM | |
Posts: 56 Rating:
|
Dear dayanada, Please find below details & as well as link. http://support.automation.siemens.com/WW/llisapi.dll?query=6SL3462-1CC00-0AA0&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=csius&objaction=cssearch&searchinprim=0&nodeid0=4000024 Theset of four distance bolts has been introduced using order number 6SL3462-1CC00-0AA0 (originally intended for the 75 mm wide assembly bracket). Two distance bolts are required to installthe 50 mm wide modules and four distance bolts to install the 75 mm wide modules. When using distance bolts, the front of the Booksize CompactModules is located at the same level as the Booksize Modules so that the dc links can be directly connected via the integrated dc link busbars. The length of the distance boltsis only correct when using Booksize Modules and internal air cooling. The order number 6SL3462-1CB00-0AA0 for the 50 mm wide assembly bracket is not listed in the PMD and will no longer be displayed in future catalogs. Regards, Shank |
10/9/2012 4:41 PM | |
Joined: 5/6/2010 Last visit: 1/29/2023 Posts: 89 Rating:
|
Does anyone know the spacing that is created? Is it 46mm of difference between a booksize versus a compact booksize? |
Follow us on