10/6/2022 5:47 PM | |
Joined: 2/25/2022 Last visit: 2/20/2023 Posts: 7 Rating:
|
I appreciate your reply. I've checked that, and we're talking about 611A model, I've attached pictures of it down below. By the way, this drive is driving an 1PH7 105-2NF02-0BA0 Spindle Motor. Best Regards. Attachmentsimodrive pictures.docx (100 Downloads) |
10/6/2022 5:49 PM | |
Joined: 2/25/2022 Last visit: 2/20/2023 Posts: 7 Rating:
|
I appreciate your reply. I've checked that, and we're talking about 611A model, I've attached pictures of it down below. By the way, this drive is driving an 1PH7 105-2NF02-0BA0 Spindle Motor. Best Regards.
Attachmentsimodrive pictures.docx (95 Downloads) |
10/6/2022 11:02 PM | |
Joined: 10/17/2007 Last visit: 3/19/2023 Posts: 3276 Rating:
|
Not 611A --you have 611U. U means universal --it can set to use digital (from profibus ) and can set to use analog. I think you use analog--setpoint from 56/14 (56A/14A--it is double axis controller , you only use A-axis ) now you question: #1--I want you try to understand by yourself--attached picture for all enable terminals. you need read and try , give me basic idea, I will give your final summary--in this way you will never forget #2--Don't use same idea as VFD to think about servo drive --normally SIMODRIVE running with CNC or PLC controlled (AO module ) change spindle rotation direction --by change reference setpoint polar --such as from +9VDC change to -9VDC
AttachmentTer_663_65.pdf (95 Downloads) |
Please Help me to understand your question! |
|
10/7/2022 4:00 AM | |
Joined: 4/23/2010 Last visit: 3/19/2023 Posts: 8019 Rating:
|
65.A - Is A drive controller enable. 65.B - Is B drive controller enable. 663 - Is Pulse enable (IGBT) Please refer SIMODRIVE 611 universal SIMODRIVE 611 universal E, Control Components for Closed–Loop Speed Control and Positioning manual for more detail information. |
10/7/2022 5:00 PM | |
Joined: 2/25/2022 Last visit: 2/20/2023 Posts: 7 Rating:
|
Thank you PISCEAN. Things are getting clear now.
|
10/7/2022 8:53 PM | |
Joined: 10/17/2007 Last visit: 3/19/2023 Posts: 3276 Rating:
|
Can you use "to Thanks" button under my answer. and Forum management will marked this topic "Solved" Very appreciated for your quick response give some tips for you. I attached the page of all enables terminals --not only for the drive . but also for the power supply module. 63, 64, 48 , 112 , you should remember all of them.--attached pic for you PS: for 56/14, 63,64,65 Siemens kept using them AS SAME FUNCTION crossed generations. From SIMODRIVE 610/650 in mid of 1980 to 611 in early 1990 and 611A in 1992, 611D in 1996 and 611U in 1998--I have been used all kind of these drive systems, so which is easy for me to remember them.
AttachmentE-R_mod_enables.pdf (100 Downloads) |
Last edited by: nulizhang at: 10/07/2022 21:12:38Please Help me to understand your question! |
|
This contribution was helpful to
1 thankful Users |
Follow us on