Industry Online Support
Technical Forum
6/13/2010 1:33 PM | |
Joined: 1/19/2008 Last visit: 2/9/2025 Posts: 992 Rating:
|
HI, Only GA3 versions had the option to output the message file. If it exists it is probably in the initial clear mode. |
6/14/2010 7:10 AM | |
Posts: 2964 Rating:
|
Hello.... If you have PCIN / WINPCIN software installed you can take the backup. for that you need to make settings in your laptop as well in the system too.... EVEN PARITY, 2 STOP BITS,7 DATA BITS,4800 BAUD RATE,DISPLAY ON,DIRECTORY ON,CANCEL OFF,FILE OPT OFF,END_W_M30 OFF,ETX OFF,BINFILE OFF 5011-11000110 5013-11000110 I am also attaching you the pdf file for data loading procedure which is already posted in our technical fourm. Check it out ..... Ekalavya Attachment810_820 reload.pdf (272 Downloads) |
Follow us on