9/11/2013 7:50 PM | |
Posts: 297 Rating: (41) |
The gray code mapping is described here: https://www.automation.siemens.com/doconweb/showpdf.asp?item=7412&cd=sinumerik_simodrive_04_2010_e&scope=all&ResultSet=7413&CurrentItem=7413&ResultType=content Do you have the standard 23 position feedrate switch, or something different? If a different switch is used, then the machine parameters in MD12030 will be different than default. In any case, as you've seen, it's not easy to decode the current override setting from the switch position. If you can use the NC, you can look at system parameter $AC_PLC_OVR, or maybe $AC_TOTAL_OVR to determine the actual values. You can use synchronous actions to set signals based on the actual override. HTH, SteveA |
Follow us on