7/5/2011 2:56 PM | |
Joined: 5/22/2009 Last visit: 5/3/2022 Posts: 40 Rating:
|
hello on my system isn't VNC... to ip a.b.c.d:10 but VNC... to ip a.b.c.d:6 ? port 106 in TCP or UDP ? Or both ? I have try TCP/106 and TCP/106 UDP/106 without succes it's look that is not port 106 but 102 check http://support.automation.siemens.com/WW/view/en/8970169 but no succes with this by advance thank's |
Last edited by: phgo at: 7/6/2011 2:53 PMLast edited by: phgo at: 7/6/2011 1:46 PM |
|
2/20/2012 5:17 PM | |
Posts: 30 Rating:
|
Hello, Have you found a solution for this issue yet? I'm having the same problem and have been unsuccessful in communicating via S7 through the X130 port. |
2/21/2012 6:43 AM | |
Joined: 5/22/2009 Last visit: 5/3/2022 Posts: 40 Rating:
|
Hello I finaly use the X127 with a VPN router "EWON" Regards |
3/31/2012 8:13 AM | |
Posts: 2964 Rating:
|
Hello... Additional to the above answer there is FAQ released reagarding to the said subject Check this link http://support.automation.siemens.com/WW/view/en/59715134 Regards, Prakash |
2/17/2017 2:06 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by jkrive is split to a separate thread with the subject How to set up company network for transfering NC programs form server to the sinumerik 840dsl?. Best regards |
Follow us on