Industry Online Support
Technical Forum
4/24/2012 2:47 PM | |
Posts: 2964 Rating: (484)
|
Hello....
What is the hardware are you using ?? pcu20 / pcu50.... PCU50 have Harddisk and the platfrom is WINXP.... PCU20 deosn't have any kind of HDD and the software is embedded inside the hardware itself. Ofcourse it is with Microsoft....siemens software are used with this technologies... Where ever you have harddisk you need to install antivirus....When you use your USB storage devices you need to scan your pen drive/ USB HDD when you put it in machine equipped with PCU50... Yes virus can enter if you don't scan it and...ensure you if you install the antivirus...make habit of updaing it regularly basis....then you can aviod it. check this note regarding the PCU50.3 http://support.automation.siemens.com/WW/view/en/37110053 Hope it is clear... Regards, Prakash |
This contribution was helpful to1 thankful Users |
Follow us on