Industry Online Support
Technical Forum
5/16/2006 10:02 AM | |
Posts: 3149 Rating:
|
Hi did you already have a try with the "getting started collection" http://support.automation.siemens.com/WW/view/en/19171527 http://support.automation.siemens.com/WW/view/en/19171968 nemo |
5/19/2006 3:41 PM | |
Joined: 9/5/2007 Last visit: 9/21/2022 Posts: 317 Rating:
|
Hi Eric, First thing you need to do is upgrade to any version of 2005. 2004 was just not worth the hassle. best of luck |
5/23/2006 4:58 PM | |
Joined: 5/8/2006 Last visit: 1/29/2021 Posts: 1085 Rating:
|
Hi, you can not transfer any files from the CF cardwhich is pluged in panel via smart@service. smart@serviceallowed toread the files only.There are noother possibilities to transfer the data from a panel to a PC. If you want to transfer thefiles to a PC you can only plug the card in a card reader which in connected to the PC. Bye |
5/23/2006 6:26 PM | |
Joined: 9/5/2007 Last visit: 9/21/2022 Posts: 317 Rating:
|
Hi Eric, Zak is mistaken here. Itis possible to transfer files from the CF card to PC using Sm@rtsrvice providing the two devices are connected on Ethernet of course. Also, you can get a free ftp server to load on the MP if you don'rt want to buy the Siemens solution (just Google for it) - The Sm@rtservice option is much neater though so in my view is worth the money[:)] |
5/24/2006 9:52 AM | |
Joined: 9/5/2007 Last visit: 9/21/2022 Posts: 317 Rating:
|
Hi Eric, You don't need Sm@rtservice to get data from the MP to the PC using script. I don't have an example (but maybe there's an FAQ?) because I'm no script expert but I know it's possible to read data from CSV on CF card and write this to file on the PC. It might even be better to use the 'Copy Log' function from CF card to PC, then do your file access scripting on the PC, depending on your exact requirements. |
Follow us on