9/4/2008 3:09 PM | |
Posts: 487 Rating:
|
You are allowed to create custome table on the SQL server database that comes with WinCC as long as the table is used in conjuction with the WinCC project. I have done this before in consultation with Siemens. Please check the FAQ below. http://support.automation.siemens.com/WW/view/en/23680533 |
9/5/2008 9:55 AM | |
Joined: 11/9/2005 Last visit: 12/6/2021 Posts: 487 Rating:
|
Hi Could install MySql . Eric |
Here we only work on 'no need to know basis' ,just fix whatever is wrong |
|
9/8/2008 9:16 PM | |
Posts: 168 Rating:
|
Furthermore, if you're right, I think Siemens should change the name of WinCC Optional Pack "User Archive" to "Useless Archive" hum heh hum hum heh |
9/8/2008 11:05 PM | |
Posts: 487 Rating:
|
Dimicamp, I think you are confused between database and datatable. If you add your own datatable in RT DB, it is not creating your own table. I completely agree with the FAQ. The case discussedDOES NOT have 'own database' or 'third party applications'. Also please check the link below from A&D Mall. If you do not consider official training material from Siemens as "Official" about CAL license. https://mall.automation.siemens.com/DE/guest/index.asp?aktPrim=0&nodeID=10016159&mlfb=6AV6371%2D1ES06%2D0AX0&aktTab=4&lang=en I have also havesample programs from Siemens WinCC support with custom table in RT Database.
---- |
Last edited by: JMJ at: 9/8/2008 11:23 PM |
|
Follow us on