4/2/2025 7:38 AM | |
Joined: 4/2/2025 Last visit: 4/2/2025 Posts: 1 Rating:
|
Hello! No worries—your questions are definitely not clumsy. They're actually quite insightful, and I'll do my best to help guide you through them! 1.What is the difference between SCADA and HMI?HMI (Human-Machine Interface) and SCADA (Supervisory Control and Data Acquisition) both deal with industrial automation, but they serve different purposes:
In simpler terms, HMI is a component of SCADA—it’s the user interface, while SCADA covers the full supervisory control and data acquisition framework. 2.Do I have to go to PC systems to do SCADA in TIA V16?Yes, when you use TIA Portal V16for SCADA, you typically interface with a PC-based system running WinCC (Windows Control Centre). WinCC is Siemens' SCADA system that integrates with TIA Portal, which is used for designing and programming automation projects. You will use the TIA Portal to configure and program the PLCs, and then you’ll utilize WinCC (installed on a PC or server) for SCADA functionality—this includes setting up the monitoring, alarms, reporting, and data storage. While basic HMIs can run on panels or embedded devices, SCADA systems in TIA Portal typically require a PC system for full functionality. 3.How do I transfer fault information (e.g., a thermal) to the SCADA?To transfer fault information (like a thermal alarm or error condition) to a SCADA system, you'd typically use the following steps:
Here’s a small example of what this might look like:
When the If you want to dive deeper into SCADA systems, including modernizations and best practices, I recommend checking out this article on SCADA Data Modernization. It talks about evolving SCADA systems and improving data acquisition and management, which might be valuable as you get more into the SCADA world. Hope that helps, and feel free to reach out if you have more questions! |
Follow us on