5/25/2012 11:17 AM | |
Joined: 4/11/2012 Last visit: 10/29/2024 Posts: 181 Rating:
|
A question: So this cable (6ES7901-4BD0-0XA0) can be used to "piggyback" an existing profibus line, that is already terminated from both ends. Will this cable work just as well for connecting only 2 profibus stations? A direct link from PG to PLC, with no other cables leaving from those ports? This connection would require termination from both ends of the cable, is this correct? If I only have need for direct connection between 2 stations, then I could use the cable in attachment OR the 6ES7901-4BD0-0XA0. If I want to piggyback an existing profibus line, then I can't use the cable in attachments, but I can still use the cable 6ES7901-4BD0-0XA0. Is this correct? So will cable 6ES7901-4BD0-0XA0 work for both spur-lines, and for standalone? AttachmentProfibus PG cable Self made.pdf (69 Downloads) |
Last edited by: O_Moderator at: 5/25/2012 12:36 PMnew subject after splitting from /tf/WW/en/Posts/58744#top |
|
Follow us on