6/30/2007 12:22 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hello 931221, In fact it's possible to add so called 3rd party deviceslike antennas and IEEE 802.11 a/b/g products. The addition of antennas is quitte easy. I have neveradd a third party Access Point but I think this must be more easy like adding the name, adding the power output and that's it. But after adding these devices you won't can't configure those devices with SINEMA-E that's only possible with Scalance W versions. But planning, the most important, is possible with those. Also the site survey option in the standard version is very nice and can give you a very good view on the signalstrengths through the whole plant. Moreinfo is available here: http://www.siemens.com/sinema Good luck with it. |
Best regards, |
|
Follow us on