10/19/2023 10:17 AM | |
Joined: 7/25/2023 Last visit: 11/25/2024 Posts: 3 Rating: (0) |
Hello. short question. After long search and reading all discusses on this topic I get that point. It´s not possible to read/write a single coil/boolean in a holding register. It´s possible to read/write the whole word and get the binary value through splitting the word in its 32 bits. An oder possibility to access coils/bools is by transfering them into the input/output words and than access them with the fc-codes 01, 02, 05, 15. So to acces the output bit Q70.1 we need to: 70byte * 8 Bits = 560 + 1 = 561. Thats the only way I found to get directly on the bools. Am I right? Can someone pls confirm proof me wrong? Thank u all. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/20/2023 06:58:04New subject after splitting |
|
10/19/2023 12:59 PM | |
Joined: 7/25/2023 Last visit: 11/25/2024 Posts: 3 Rating: (0) |
Okey thank u so much for helping me. It´s more clear now. |
Follow us on