5/29/2021 8:40 PM | |
Joined: 9/27/2006 Last visit: 6/1/2024 Posts: 12259 Rating: (2670) |
Hello Harry; Have you tried the code provided earlier by Mr. Berghof? Do yu understand the WinCC systm tags (tags that are preceded by "@"), and in particular the @LocalMachineName TAG? - Which tag indicates the computer name? https://support.industry.siemens.com/cs/ww/en/view/22132846 Hope this helps, Daniel Chartier |
5/29/2021 8:46 PM | |
Joined: 6/2/2020 Last visit: 10/6/2023 Posts: 215 Rating: (0) |
Hello Sir, I had tried this tag but not successful as I already configured mouse click on this toggle button. Now I just need to hide this button another OS and to show only a single OS. So I need a script for my computer name which is Bhushanfmos09. Actually I dont have a huge knowledge of C script that is why I need full script. Sir please support. |
Last edited by: Harry55 at: 05/29/2021 20:47:09 |
|
6/5/2021 12:43 AM | |
Joined: 6/2/2020 Last visit: 10/6/2023 Posts: 215 Rating: (0) |
@Goerge & Daniel Sir, I had tried to use this script to display but it wont work. Please check and suggest something. |
6/9/2021 7:40 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (216) |
Hi Harry55, in your script you have missed the @ in front of the variable @LocalMachineName. If you have problems with C- or VBS-scripts you can use the WinCC tool apdiag to debug your code. With regards |
This contribution was helpful to1 thankful Users |
6/9/2021 1:54 PM | |
Joined: 6/2/2020 Last visit: 10/6/2023 Posts: 215 Rating: (0) |
Sir, After @ , it is not working. If possible can you send me the script as I tried all these things but not working. |
6/21/2021 9:42 PM | |
Joined: 9/9/2015 Last visit: 5/28/2024 Posts: 727 Rating: (270) |
Harry, I think you at least need to show appreciation on somebody else taking time to reply your question by just clicking a "THANKS" button and "RATE" button. The their time value cost more than that. Sometimes, they don't even want to spend time in understand your question, just because of your attitude. From what I see here, an expert was supporting you for so many threads, but none of them get any rating. Seem like you find it extremely not helpful till you do not want to give any appreciation note. Just drop my comment to express my feeling. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|