6/16/2013 2:55 PM | |||||
Joined: 9/27/2006 Last visit: 2/3/2023 Posts: 11949 Rating:
|
Hello Ras; Is this a typo, did you mean a CPU 1215? If you reallyhave a CPU 215, you need S7-MicroWin to program it, you cannot use TIA Portal. And since the S7-215 is of an older generation of S7-200, I believe you must use an older version of MicroWin, such as v. 3,2.
This quote is from one of the Update files available for Microwin 32 (I the Entries tab of the link above): COMPATIBILITY: STEP 7-Micro/WIN32 Version 3.2.4 supports all S7-200 CPUs, including the 21x series (CPU210, CPU212, CPU214, CPU215, CPU216) and the 22x series(CPU221, CPU222, CPU224, CPU226 and CPU226XM at present). If you are speaking of simulation on a S7-1215, then look at this thread, specially the posts from Pegaia: |
||||
Last edited by: dchartier at: 6/16/2013 5:16 PM |
|||||
This contribution was helpful to
1 thankful Users |
6/17/2013 7:03 AM | |
Posts: 69 Rating:
|
Dear Daniel, Thank you for the help. And excuse me for the mistake. I use S7 1200 CPU. I should to try the Pegia solutions. Regards, Ras |
6/17/2013 9:26 AM | |
Posts: 69 Rating:
|
Hi, The problem was solved by the solution. Regards, Ras |
This contribution was helpful to
1 thankful Users |
Follow us on