Industry Online Support
Technical Forum
4/23/2008 12:25 PM | |
Joined: 11/15/2006 Last visit: 1/20/2025 Posts: 1319 Rating: (176) |
There is an quite good FAQ about configuring WAN Access to plcs. See FAQ 26662448 http://support.automation.siemens.com/WW/view/de/26662448 |
Have Fun! |
|
4/23/2008 1:25 PM | |
Posts: 13 Rating: (1) |
Ok, thanks you for your answers, I take note of the subject and I will keep you informed of my situation. Bye |
4/23/2008 1:28 PM | |
Posts: 487 Rating: (36) |
Hi Ici un lien en francais , its the same as from TomDeWou To be on the safe side you have to use VPN to either connect to a PC inside the factory with Step7 installed .Using VNC or Remote desktop ( if you use XP or Vista) you can then 'take-over' the factory PC Another way is to bay and install a scalance S connected to the factory intranet and then you can use your PC/PG with Step 7 from home ( still connecting via VPN) Her is another link to a french manuel Greetings Eric |
Follow us on