12/13/2016 2:02 PM | |
Joined: 12/18/2014 Last visit: 2/15/2025 Posts: 34689 Rating:
|
In my opinion, their ideas are not realizable. Edit: Only modifying of some Parameters of the 0BA8 via VM is possible. AttachmentLOGO! 8 - Industrial Ethernet LOGO! CMR2020 _ LOGO! CMR2040_Edition_2015_05 pages 11-14.pdf (365 Downloads) |
Last edited by: ixo65 at: 12/13/2016 2:04:58 PM |
|
12/13/2016 2:28 PM | |
Joined: 12/18/2014 Last visit: 2/15/2025 Posts: 34689 Rating:
|
Do you not think also if your ideas were realizable, that this would be in the description? |
12/13/2016 8:11 PM | |
Posts: 3 Rating:
|
Indeed.. anyway, thank you for the answer! |
This contribution was helpful to
1 thankful Users |
12/16/2016 9:17 PM | |
Joined: 12/13/2014 Last visit: 2/14/2025 Posts: 151 Rating:
|
I have assumption that this IS possible (but not yet tried by myself): CMR2020/2040 manual, page 17 In addition to this you can use OpenVPN for direct communication with the BM if the CMR is entered as a router with the BM. This means on base module IP settings CMR2020 must be set as BM gateway. And functional enchancements says: As a result, access is possible to the websites of the LOGO! basic module. is possible using LOGO! APP. is possible using LOGO!Soft Comfort for uploading/downloading the program to/from the LOGO! basic module. ------Another problem can arise, when trying to access BM via CMR2020 (over GPRS). Many phone service providers blocks incoming traffic and can charge extra fee for enabling direct access. As CMR20X0 provides only OpenVPN server and not client, then your device (PC, tablet or smartphone) as client side must initialize establishing connection with server (CMR20X0). So you must know CMR20X0 WAN side IP address (or use payable dyndns service) _AND_ CMR20X0 SIM owner (phone service company) must enable direct access to CMR20X0. All will be easier, if Siemens adds OpenVPN client functionality too. |
Last edited by: WWEE at: 12/16/2016 9:19:01 PMLast edited by: WWEE at: 12/16/2016 9:34:59 PM |
|
This contribution was helpful to
2 thankful Users |
4/14/2017 11:31 AM | |
Posts: 1 Rating:
|
Hi Thomas, Regards xin |
Follow us on