10/30/2012 9:28 AM | |
Posts: 1547 Rating:
|
Hi, the DCOM configuration is a complex terrain. I suggest to have a look in the manual "SIMATIC NET Industrial Communications Commissioning PC Stations - Manual and Quick Start " under http://support.automation.siemens.com/WW/view/en/13542666.In chapter 4.7 you'll find a configuration guide. For testing you should try to use the OPC Scout on the WinCC Server pc at first (instead of WinCC as OPC client). It would also be helpful to deacitivate the firewalls on both pcs (for testing only). Perhaps the usage of OPC UA could be a option for you? With this mechanism you don't need to make such settings as a DCOM configuration. |
11/6/2012 4:31 AM | |
Posts: 32 Rating:
|
Thank you for your support.......... Its started communication after adding remote access permission for the user "NETWORK" . |
Follow us on