11/13/2006 6:57 PM | |
Posts: 1084 Rating: (72)
|
Looks to me that you have more then 5000 actions running at the same time. |
11/14/2006 10:20 AM | |
Posts: 3149 Rating: (171)
|
Hi perhaps this FAQ can help as well http://support.automation.siemens.com/WW/view/en/2357302 nemo |
11/14/2006 11:47 AM | |
Posts: 1084 Rating: (72)
|
Thanks Nemo, I have a day off I think, forgot even to look in the faq myself... with regards, Ikkezelf |
11/14/2006 12:05 PM | |
Joined: 3/8/2006 Last visit: 4/10/2024 Posts: 15 Rating: (4) |
Sorry I didn't take the log file, but as I can see, there was no special message in it. If you really need them, I can ask my customer to send them to me. I don't know if it could help, but in the WinCC application there is an action with notrigger. Normally this action should not be activated, but does the system always used it ? To answer Nemo,the FAQ "http://support.automation.siemens.com/WW/view/en/2357302"seem not to be helpful. All my scripts or actions are at least used onceper day. And none of them generated an error. Whatever the moment of starting, the script blocks after exactly 2147483647 ms. Best regards, |
11/19/2007 3:25 PM | |
Posts: 1776 Rating: (95)
|
first check the diagnostic files, use apdiag and so on see diagnostic cluster in the FAQs http://support.automation.siemens.com/WW/view/en/22892165 |
1/14/2008 2:24 PM | |
Joined: 2/22/2006 Last visit: 2/17/2024 Posts: 73 Rating: (3) |
Hi, here are the logs from my test-pc. As it happens on this pc too, I think the problem is within the project and not on the pc. You don't have any incompatible software in those computers, right? >> I don't think so. You said the projects have the same "base engineering"... does this mean someone created a project, then you deleted the data from the old project to start this one? Or do you have a basic application, with basic features, and use it for all projects? >>once we made a project, and for the next one we took the old and modified it, ... Were all projects created / edited under the same WinCC version? >>Starting was with V60+SP2, now the two projects with this failure ar V60+SP3 and V60+SP4. You said you think you think it's a 24 days interval... Do all computers fail at the same time, or do they fail with the same time interval? >>It's not always this intervall. On my test-pc the break was after 2 days, and now it is running since 10.1. Thanks AttachmentPIO5000.zip (110 Downloads) |
Last edited by: Franschitz at: 14.01.2008 14:27I've forgot one think: what is the CCRtsLoader.exe? |
|
3/7/2008 7:09 PM | |
Posts: 1275 Rating: (123)
|
Hi, Have you tried contacting technical support for this? They may help! Best regards, Danielle |
3/11/2008 12:35 PM | |
Posts: 1275 Rating: (123)
|
OK... Please let us know how that works! Good luck.. Danielle |
3/14/2008 10:40 AM | |
Posts: 20 Rating: (2) |
Hi, Franschitz. Here is the archive with log-files. There are a lot of them, so you can check OPC_01.LOG and WinCC_Sys_01.log in cppn folder, there is some information about connection errors. There are also messages like "ArchiveManager,Failed to switch archive(Type:1):(null)" in file WinCC_Sys_01.log in folder srv2. The last hang of computer srv2 was at 13th of january, and there is no messages in log files about this at all. Support hotline recommended me to install some diagnostics software, which creates huge log-files (about 100 Mb) every several minutes. I think it's dangerous to use it in production environment, especially if there is no qualified personnel at site. Best regards, Alexander. AttachmentDiagnose.zip (104 Downloads) |
Last edited by: Akorostel at: 3/14/2008 11:25 AM |
|
3/14/2008 11:11 AM | |
Joined: 2/22/2006 Last visit: 2/17/2024 Posts: 73 Rating: (3) |
I think you forgot the attachments |
3/14/2008 11:26 AM | |
Posts: 20 Rating: (2) |
oops... Please have a look at the updated post. |