6/28/2015 12:27 PM | |
Joined: 11/29/2014 Last visit: 1/24/2023 Posts: 82 Rating:
|
hello every body i have one motor in production line and it's encoder pulse is very bad.i did very attempt to improve and solve it but problem is there yet.i send 3 picture about it.can every body help me?how can i get the suitable signal from encoder?it should be mentioned in that line,there is some other motor but it's encoder pulses are ok and just this motor has problem. best regard mohsen bagheri Attachmentgraph.docx (118 Downloads) |
6/30/2015 7:42 PM | |
Posts: 87 Rating:
|
Hi. Which siemens drive are you using? It is possible make a test in vector mode with encoder less? How did you the optimization? Regards.
|
7/1/2015 1:31 PM | |
Joined: 11/29/2014 Last visit: 1/24/2023 Posts: 82 Rating:
|
hi when i disconnected it,i did measurement (auto tunning) again. load is not roller press,just roll is rotating and move the sheet in line. drive chains are ok. I uploaded the actual trace file here,if you check the trace file;you see just in some speed problem is there and in other speed it 's ok. regards Attachmenttrim.rar (90 Downloads) |
Follow us on