8/1/2018 7:47 PM | |
Posts: 2 Rating: (0) |
I have a Sinamics V20 Drive 6SL3210-5BE24-0UV0 mounted inside a small electrical enclosure. I would to add a momentary push button on the exterior of the enclosure and wire it to the V20 in order to reset any fault on the drive fault without getting into the enclosure. Where would it wire the push button onto the drive? What parameter(s) would need to be changed for this function? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/2/2018 12:25:34 PMNew subject after splitting |
|
8/3/2018 5:31 PM | |
Posts: 2 Rating: (0) |
Thank you. I will get this wired and tested. thanks again. |
Follow us on