12/5/2012 8:45 AM | |
Posts: 3037 Rating:
|
Hello Alec Tek, You can use 32 connection to DP-Slaves with WinAC MP 377. See chapter A. SIMATIC WinAC MP 2008 For communiction with profibus see chapter 3. How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? You can use a MP377 for profisbus communication or you can use another panel that you can use on profibus. Tweety |
12/5/2012 12:12 PM | |
Joined: 9/27/2006 Last visit: 2/17/2025 Posts: 12337 Rating:
|
Hello Alec; According to this FAQ, you should not have trouble installing a new panel on your system: Number of Operator Panels on a WinAC MP V3.0 SP1 QUESTION: ANSWER: What kind of error do you face in setting up a new panel? Hope this helps, SIMATIC HMI Panels - Brochure, November 2011 |
Follow us on