5/31/2022 2:12 PM | |
Joined: 10/21/2016 Last visit: 10/31/2023 Posts: 49 Rating: (0) |
Hi, did you resolve the problem? I have encountered the same doing some modifications inside Multiproject taken from site. I added new AS with ET200SP and some I/O modules - for all of them I have a problem with " No hardware found for... ". ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/01/2022 10:01:47New subject after splitting |
|
6/8/2022 8:20 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi hubertluczak, the interface module 6ES7 155-6AU01-0BNO is not released with PCS 7 and can't used with generation of module drivers, no matter which I/O module do you use. Every hardware device which you want to use the generation of module drivers have to be in the PCS 7 catalog and all other wouldn't work. So before you want to buy a hardware component for a PCS 7 project have a look at the manual PCS 7 Released modules (for example see the interface module of ET 200SP IM), because there you can find all hardware components that will be supported the generation of modules driver in PCS 7. Just as hint. You can use all other devices from Siemens or other manufacturer (by adding a devices with GSD-file) in PCS 7 and get information or control the device, but you can't use the integrated devices diagnostic of PCS 7. And your error message I haven't see before. Can tell us what you did and send a screen shot of the error message? Is the error message is coming from the HW config or from the CFC compiling? With regards |
7/10/2022 9:49 PM | |
Joined: 10/21/2016 Last visit: 10/31/2023 Posts: 49 Rating: (0) |
HW config attached. Server module on last position. |
Last edited by: hubertluczak at: 07/10/2022 21:49:57 |
|
Follow us on