5/5/2023 9:24 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello solanome You could use the alarm system of WinCC... create descrete alarms and use in the alarm text a textlist field or also tag values -> in the Alarm Log /alarmView you would be able to see what happend Or you would use a script for writing the needed information in a csv File. In a script you can use the systemfunction LookupText to read out a specific text from a testlist. Table controls are not implemented in WinCC Comfort/Advanced. In the Toolbox is a workaround with simple screen elements and scripts: https://support.industry.siemens.com/cs/de/en/view/106226404 Bye Murof |
Last edited by: Murof at: 05/05/2023 09:25:09If this Information really helps, you could use the Rate function |
|
Follow us on