9/23/2017 3:12 PM | |
Posts: 3 Rating:
|
Hello, It is also possible with wincc confort V14 SP1 to put the text list in the property of the faceplate. It is not the case with Wincc pro V14 SP1, the text list can only be create Inside the faceplate. If I use the same text list for different faceplate inside my project, when I modify the text list I have to modify all my faceplates. Is there a solution to have the same principe than with the WinCC confort V14 with WinCC Pro? With script? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/26/2017 6:12:19 AMNew subject after splitting Last edited by: BenoitImeca at: 2/21/2019 11:14:49 AMLast edited by: BenoitImeca at: 2/21/2019 11:15:40 AMLast edited by: BenoitImeca at: 2/23/2019 6:45:57 PM |
|
Follow us on