6/25/2018 2:58 PM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello, ok and how you did HW cfg of Profibus? Also some Step7 requirements must be ok for cfg. You can look to this manual: CP345-5 Manual B |
Last edited by: Duris_I at: 6/25/2018 3:09:17 PMWith best regards... |
|
6/25/2018 3:02 PM | |
Joined: 1/27/2009 Last visit: 3/19/2025 Posts: 172 Rating:
|
This is my hw configuration file.Attachmenthw.zip (62 Downloads) |
The only thing necessary for the triumph of evil is for good men to do nothing |
|
6/25/2018 3:09 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello Arturas; Please have a look at the following document, it describes the differences between an integrated DP port (on a CPU 314C-2DP, for example) and a CP 342-5 as DP masters. The step-by-step description should help you prepare the configuration and the setup of the required functions DP_Send and DP_Recv (for the CP 342-5): What should you watch out for when configuring a CP342-5 as DP master and why is it necessary to call the FC1 'DP_SEND' and FC2 'DP_RECV' functions in the user program of the CPU in order to transfer data? https://support.industry.siemens.com/cs/ww/en/view/18208090 Hope this helps, Daniel Chartier |
This contribution was helpful to
2 thankful Users |
Follow us on