9/24/2018 6:40 PM | |
Joined: 9/3/2008 Last visit: 3/24/2025 Posts: 933 Rating:
|
Hi Ahmed, Did you compare the settings on the new computer to the old computer as suggested in one of your other threads? NB: Please try not to make multiple questions on the same issue. This makes helpful people start from scratch trying to make suggestions when they have already been suggested (without knowing if it was followed)... Also, as Murof says... give all necessary information about your setup please, as was also asked for in one of the other threads... |
Last edited by: Michael K at: 9/24/2018 6:41:45 PMMichael |
|
9/24/2018 9:32 PM | |
Joined: 11/26/2016 Last visit: 10/8/2023 Posts: 138 Rating:
|
Hi Mechael, I have a big problem and I have to solve it in Wednesday, I have only 7 houres to solve it, and I make these question to get the solution in a short time. Iam no intended to get more posts, but my problem related to many sections as pc, network, tcp, scada...etc, excuse me I haveva big problem. |
Last edited by: E.Ahmed at: 9/24/2018 9:36:50 PMLast edited by: E.Ahmed at: 9/24/2018 9:39:03 PMNothing IS IMPOSSIBLE. |
|
9/27/2018 10:31 AM | |
Joined: 8/3/2009 Last visit: 3/27/2025 Posts: 15095 Rating:
|
Hello E.Ahmed How does this "promotic v7" scada system work together with the Siamtc Net configuration ? If you use SIemens HMIs then you also have to set the PGPC Settings in Windows Control Panel and if you use a Station Configuration then you have to set it to an internal Setting. If you do not use this then you have to set the virtual Access Point to a Hardware access Point. I Would contact the Company of the Promotic V7 Scada System. they should know how to set up their Software. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on