8/4/2020 3:06 PM | |
Joined: 10/11/2006 Last visit: 4/24/2024 Posts: 5823 Rating: (789)
|
Hello, superimposed is a possibility. 3.14 Superimposed motion https://support.industry.siemens.com/cs/ww/en/view/109767619 3.14 Superimposed motion Superimposed motion is defined with mergeMode=SUPERIMPOSED_MOTION_MERGE. Superimposed motions are independent motions. Superimposed motions cancel each other. Superimposed motions can be stopped and continued separately. Superimposed motions on a position axis are executed in the superimposed axis coordinate. 3.13.10 Superimposed positioning Superimposed positioning is performed in the superimposed coordinate system of the axis. The target position can be specified as an absolute or relative position in this coordinate system. (For feedback of the target position, see Superimposed motion) The superimposed motion has its own programmable dynamic response parameters. The userDefault settings of the dynamic response parameters are identical to the settings of the main motion. Blending conditions for the superimposed motion are ignored.
|
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on