10/9/2024 5:41 PM | |
Joined: 5/6/2022 Last visit: 2/10/2025 Posts: 551 Rating:
|
Hi Fueguinhio, It is not nessecary and not possible to transfer the audit license to the Unified panel. You do not need it directly on the panel. The only thing you need to be able to use Audit on the panel is the Audit certificate. You can create this on your PC using the Unified certificate manager. Then you can export the device you created with the certificate to a panel via a USB drive and import the certificate. It is nessecary to enter a password and remember the iteration number upon exporting and importing the certificates. You can have a look at the following SIOS entry for the use of certificates with WinCC Unified: https://support.industry.siemens.com/cs/ww/en/view/109828368/155440602379 You can have a look at the following entry for the import of certificates into the panel: https://support.industry.siemens.com/cs/ww/en/view/109826164/173477261195 Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on