8/20/2011 8:57 AM | |
Posts: 1 Rating:
|
Hi everybody, Recently, I've loaded a program to S5 135U CPU 928B. The program has downloaded succefuly and for the first time the PLC has runned with a cold Restart. But for the other times also I shoud use a cold restart and now I have another problem. PLC don't run and it gives an ADF error. I've deactivated the OB blocks from OB 23 to OB34 with DX0. After this, PLC ran but with some problems and many function of the machine didn't work. In addition some of the output didn't activate. I've tried the ISTAK but I couldn't interpret it very well. I think one of the I/O has some problem. How can I find that I/O module? Funny thing is, sometimes it runs with cold restart but other times it gives the ADF error. I don't know what should I do? For better comprehension, The main rack has these units: "6ES5525-3UA21" , "WE706 6FM1706-3AA00" , 9 input modules , 6 output modules , "6ES5 308-3UA12". In addition it has 5 extension ET100 unit. First one has 3 input and 7 output card.Second one has 4 input and 4 output and one analog input.Third one has 3 input and 7 output.Forth one has 8 input and 3 output.Fifth one has 8 input and 3 output. I've attached the ISTACK pages when the ADF error has happend. I'm really appreciate in advance any responses. AttachmentErr ADF Led.zip (116 Downloads) |
3/20/2015 6:52 AM | |
Joined: 4/5/2006 Last visit: 1/12/2023 Posts: 642 Rating:
|
Hello, if you have a programming device then post screenshots from the stacks. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster with innovative PLC-Tools |
Follow us on