7/16/2024 6:56 PM | |
Joined: 7/7/2010 Last visit: 9/5/2024 Posts: 15143 Rating:
|
Have you ever adjusted the working pane zoom level from the default of 100% to say 90% and see how that seems to improve screen layout. To my eyes, switching from 100 to 90% does not change every rendered item on the screen the same zoom level. For example, LAD rungs do not shrink much, but the LAD components (NO/NC contacts, MOV / ADD / SUB / coils) seem to squeeze smaller relative to the rung portions. Just a thought. Have you considered modifying your programming "style"? I find if you use tag names in camelCase rather than "spaced out tags" and compared to Tags_Where_Underscores_Replace_Spaces render differently, and Portal decides differently when to split tag name whether its no spaces or underscores compared to spaces / underscores. If you stick with the S7-1200/1500 Programming and Style Guidelines at least you will be dealing with the same issues Siemens own developers and programmers deal with when they create Libraries, sample applications, and so on. And in that situation, change is more likely to happen and improve or at least change rendering of tag names in the working pane.
|
science guy |
|
Follow us on