11/3/2017 3:34 PM | |
Posts: 8 Rating:
|
Hello, I have a similar problem: I have Hercules listening as TCP server. As soon as Hercules start listening I have status 7006 and BUSY bit goes true. TCP Port and IP address are ok. Have tried to play with AdHoc parameter true or false, but this doesn't change. Is my data correct (array[0...999] of Char) ? What am I doing wrong ? TIA Portal is V13 SP2 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/6/2017 11:30:01 AMNew subject after splitting |
|
11/4/2017 2:25 PM | |
Posts: 8 Rating:
|
Ok, thank you for the replies Problem still remains I have made a pdf with some screenshots I have tried with adhoc parameter set as true and false, but same problem. A m I doing something wrong here ? Btw, I can send data (string) from PLC to Hercules on PC with the TSEND_C instruction AttachmentTCP Receive function PLC.pdf (258 Downloads) |
11/4/2017 2:27 PM | |
Posts: 8 Rating:
|
Informatively, in annex a screenshotof the connection parameters of the block |
11/4/2017 2:36 PM | |
Joined: 4/28/2015 Last visit: 3/26/2025 Posts: 10837 Rating:
|
Hello, maybe you can set LEN parameter of TRCV_C to 65535. |
With best regards... |
|
Follow us on