8/9/2017 10:33 AM | |
Joined: 11/20/2013 Last visit: 4/24/2024 Posts: 25 Rating: (1) |
Hello I have faced the same problem in 3 different occasions. I have checked the power supply, grounding and pins of Rack and found all of them are ok. I also did frimware update to latest available version. But then also this problem appears after a gap of 15-20 days. Then after complete memory reset the problem disappears and the CPU runs successfully for another 15-20 days and the problem appears again! I have collected the diagnostic buffer of the faulty CPU by putting the toggle switch to Stop and making a memory reset which I'm attaching herewith but have no idea what is the source of this problem and how this can be arrested? ------------------------------------------------------------------------------------------ AttachmentFaultyCPU.zip (140 Downloads) |
Last edited by: Jen_Moderator at: 8/9/2017 10:58:10 AMNew subject after splitting |
|
8/9/2017 10:46 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, what CPU are you talking about? In your attachment are two diagnostic buffers. one from a 319F and one from a 414. I guess your query is about the CPU414 with the diagnostic buffer entry :
Try a FW-update. Some kind of those errors are described there in the FW-update-notes. Download Operating System Updates V4.5H CPU412-3H / CPU414-4H / CPU414-4H PG / CPU417-4H If the situation is not better with the latest FW, I would create a Support Request to contact Siemens directly. hope this helps, regards, |
FCK WAR! |
|