Industry Online Support
Technical Forum
8/22/2011 7:41 AM | |
Joined: 9/28/2005 Last visit: 12/10/2024 Posts: 2957 Rating: (243) |
Hello all, I have no possibility to test it right now, but maybe someone did this. So does this issue http://support.automation.siemens.com/WW/view/en/46163827 applies to V11 also or was it solved in V11 ? |
Best regards, |
|
8/22/2011 11:36 AM | |
Posts: 267 Rating: (24) |
Hello Darius, it is solved in V11. But you need the PID_Compact >=V1.1 for firmware >=V2.0.
Please have a lookat "Bild 16" of http://support.automation.siemens.com/WW/view/de/46163827 and in the help of V11 -> PID_Compact -> Input parameters -> Reset parameter. Regards, |
This contribution was helpful to1 thankful Users |
Follow us on