3/12/2016 1:51 AM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684)
|
Hello ablo;
I have no experience with AGV positioning myself, but I contacted one of my friends working with such an application in his warehouse project. He says he is testing P+F PGV100-F200A-B16-V15B optical reading heads for AGVs, with a Profibus-DP interface and able to read Data Matrix codes. The reading heads work pretty well for him, seem to be robust and easy to integrate in his control system (not Siemens, though). Here is a link to the P+F webpage for these positioning sensors: http://www.pepperl-fuchs.us/usa/en/classid_3334.htm?view=productgroupoverview Hope this helps, Daniel Chartier
|
Last edited by: dchartier at: 3/12/2016 3:16:29 AMLast edited by: dchartier at: 3/12/2016 2:38:26 PM |
|
3/12/2016 7:31 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello, or contact experts, they have big experience with this bussines :) http://ceittechinnovation.eu/index.php/en/ Maybe they give you relevant info also. |
With best regards... |
|
3/12/2016 11:02 AM | |
Posts: 18 Rating: (0) |
Many Thanks Duris_I, I will keep your details |
3/12/2016 3:59 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684)
|
Hello Pablo; Sorry, since my friend is in testing mode, he feels he cannot disclose much more information. He suggests you use P+F technical support for more help, he finds it helpful. Here is the link to P+F North America support: http://www.pepperl-fuchs.us/usa/en/24.htm There are links to other worldwide contacts if required. Hope this helps, Daniel Chartier |