Industry Online Support
Technical Forum
5/24/2007 4:37 PM | |
Posts: 1084 Rating:
|
Hi, what do you mean with locking the alarm groups and taglogging? |
5/24/2007 9:19 PM | |
Joined: 12/5/2005 Last visit: 8/30/2023 Posts: 239 Rating:
|
Hi, You can use the function TLGLockArchiv to enable or disable the acquisition of a archive, by archive name. See the faq: http://support.automation.siemens.com/WW/view/en/218573 For lockgroup messages exists the function MSRTLockGroup. Its necessary an HANDLE of MsgService to use this function. You can get a HANDLE of MsgService using the function MSRTStartMsgService, when the HANDLE be not more necessary, you will have release him using the function MSRTStopMsgService. Well, see the project in attachment file. AttachmentCC_LockMsg.zip (73 Downloads) |
Márcio Santos |
|
Follow us on