10/5/2021 9:55 AM | |
Joined: 8/9/2013 Last visit: 12/10/2024 Posts: 1 Rating: (0) |
Hi, Thank you for this. Once one or more alarms are triggered and the count goes up it never seems to go back down. Even when the alarms have cleared. Please can you help with this? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/05/2021 13:17:44New subject after splitting |
|
10/5/2021 7:03 PM | |
Joined: 7/2/2015 Last visit: 6/21/2024 Posts: 96 Rating: (23) |
Dear KPersse, Do you have the last panel version? You can check the last panel versión at the following link. Do you have the las engineering software version? You can check the last v16 update at the following link and the last v17 update at the following link. |
If this Information really helps, you could use the Rate function |
|
10/6/2021 6:52 AM | |
Joined: 10/5/2020 Last visit: 10/10/2023 Posts: 82 Rating: (10) |
Hello, please share the script that you're using to count the alarms. |
Follow us on